Search Help




Clipsal Fire Tek Smoke Alarms are a small investment for your customers, considering they protect their most valuable assets; family, friends and home.
The high-quality, robust electronics are designed for reliability, to ensure early detection and warning from hazardous smoke and fire. All Clipsal Smoke Alarms incorporate photoelectric detection technology, which reliably detects smoke from smouldering fires – the most common and highest risk type of fire in residential environments.
The Australian Building Code mandates all new homes must have AS3786:2014 compliant smoke alarms installed.
The Clipsal smoke alarm portfolio includes surface mounted smoke alarms as well as a flush mounted smoke alarm.
Description of the complete range of smoke alarms including technical data.
Detailed technical description and technical data of the 755LPSMA4