Promote & Sell
Search Help




Demo Site
Experience by Offer or Segment, complete with supporting promotional materials.
Licensing Portal
Smart tools to support the quotation, ordering, and commissioning of Power Operation.
Community
Tap into the PSO ecosystem to discuss issues and find answers.
Training Academy
Access important training for you and your team for all Digital Power offers.
Self-paced curriculum takes you through the journey of a Power Operation Project Deployment through interactive videos.

→ Connect now to mySchneider to discover the EcoXpert content ←

Extensive details about the Power Operation software offer are available in these powerpoint presentations, including the latest release of EcoStruxure Power Operation – which strengthens its position in edge control market space and is an important step forward for EcoStruxure Power. More than a SCADA system for power networks, version 2022 is designed to work as an open platform, with high-speed control capabilities and the latest cybersecurity enhancements.

Why upgrade to the latest version of Power Operation 2022? Find out here!

Detailed presentation that covers value propositions and case studies of Easergy P3 and PME or EPO systems, including arc flash applications and more.

URL: Power Management solutions | Schneider Electric Global (se.com)
User name / password: demo / demo

PMCS Short Form Specification - [External] 2022 technical specification document for the product designed to be included in a short form specification
PMCS Short Form Specification with Killing Phrases Highlighted - [Internal] 2022 technical specification document for the product with highlighted killing phrases
Killing Phrases - [Internal] 2022 document that describes the customer value and differentiation for the killing phrases
Edge Control meeting needs of Mission Critical Facilities - Power Operation presentation for consultants

eBrochure - Share this interactive eBrochure with your customers for a dynamic overview of Power Operation 2021, its value propositions, applications, pertinent segments and the advantage of EcoStruxure Power
Flyer - View the one-page fact sheet for Power Operation 2021 features and benefits
Press Release - Announcement of the new EcoStruxure Power Operation 2021, perfect for mission-critical power applications
Social media - Posts and event support for the EPO 2021 launch and beyond. Includes images, message matrix per social channel, and hashtags to get the message out Coming soon!
Offer Banner (kakemono) - For the EPO 2021 launch for tradeshows and other events
Web Banners Animated banner ads - Graphics in 3 sizes to support your campaign and attract traffic to your SE web pages for the EPO 2021 launch

Guidelines for the availability of support throughout the life of Power Management Software products including PO and PME. Updated November 2025.

Discover extended functionality for edge control platforms, choose your application presentation below.
Click to download these module overviews:

Comparison of Power Operation to similar offers from other vendors. Updated as of April 2022

Positioning of Power Operation with other Schneider Electric and Aveva offers.

Certificates of compliance to IEC 62443-4-1 and IEC 62443-4-2 Security Level (SL2) for Power Operation
IEC 62443 4-2 SL2 Press Release
Certificates of compliance to ISO 50001, ISO 50002 and ISO 50006
ISO 50001, 50002 and 50006 Certifications for PSO with Advanced Reporting
DNV UCAIug “IEC 61850 Certificate Level A” certificate and verification report
IEC 62443 3-3 SL1 system certification for Large & Critical Buidlings

Official statement describing the country of origin for both PO and PME.
PO and PME Country of Origin Statement
Official statement indicating that Power Operation is same offer as what was previously known as PSO, PSE and PLS.