Essential Materials
Search Help





Product Announcement - Overview of the new offer value proposition, benefits and features, product information, training and contact information.
PA-00861 - SpaceLogic Wireless Connectivity – Advanced for EcoStruxure Building Operation 2022.
PA-00842 - New Service for Adding Zigbee Device Support to Ecostruxure Building Operation.

Promotional Materials
Internal Overview Presentation - Internal presentation highlighting the new offer value, features, compatibility, and device support.
Value-Based Proposition Pitch Deck - Client-facing presentation highlighting the value proposition, features and benefits.
Value-Based Proposition Video - Client-facing video recording highlighting the value proposition, features and benefits.

Applications Brochure - Brochure explaining five use cases for SpaceLogic Wireless Connectivity – Advanced, including descriptions and system architectures.
Supported Zigbee Devices Brochure - Overview of the Schneider Electric and 3rd party wireless connectivity supported devices, including description, applications, values and benefits.
FAQ - Frequently asked questions about SpaceLogic Wireless Connectivity – Advanced.
Support Inquiry Form - Download and complete to request support in EBO for new Zigbee wireless devices that are not currently supported.

EcoStruxure Building Operation 2023: SpaceLogic Wireless Connectivity – Advanced
(MLL Course Code BLDBMSE0001097)
Learn about EBO SpaceLogic Wireless Connectivity – Advanced support, how the SpaceLogic USB Wireless Adapter allows wireless connectivity on the EBO Platform, Zigbee workflows in SpaceLogic Zigbee Coordinators (RP Controllers & Automation Servers), configuring & commissioning of supported wireless devices, understanding Standard and High Security Zigbee networks, and what a Trusted Device is and how to commission it, as well as Zigbee device import files.