Search Help




Today customers expect more than a pure lighting. Independent of new or refurbishing of existing buildings the investor expects to get more. Use this as a chance to surprise and convince your customers with a new dimension of lighting. One premium device and 2 standard devices enable you to propose the right solution for your customers.
Together with modern DALI DT8 LED-lamps System integrators can achieve:
This presentation introduces the new KNX DALI-Gateways Basic as a economic alternative of the premium device. It shows especially the new dimensions of colour control via KNX and DALI but also the other functions like direct manual operation, easy lamp replacement, use of the scheduler etc.
This application description show detailed the possibilities and how to select. It is not needed to read from A to Z but it is useful as a reference book for new functions here especially the various colour control possibilities via KNX.