PSO 2020

PSO 2020

Software Package

Release Date Notes
PSO 2020 R2 ISO 2020-Sep Installation media for PSO 2020 R2
PSO 2020 Release Note 2020-Sep Release Note for PSO 2020
PSO 2020 R2 Cumulative Update #3 2022-Aug Cumulative Update 3 for 2020 R2 contains all updates from CU1 and CU2. Requires at least PSO 2020 R2 to be installed prior to applying PSO 2020 R2 CU3
PSO 2020 R2 Cumulative Update #3 Hotfix #1 2023-Jan Hotfix #1 for PSO 2020 R2 CU3. Resolves WebHMI issues introduced in PSO 2020 R2 CU3.  Requires PSO 2020 R2 CU3 to be installed prior to applying update
ETL 6.2 for data exchange with PME 2020 2021-Mar ETL tool to share Power Operation historical data with PME
Language packs for PSO 2020 R2 2021-Mar Installers that can be applied to PSO 2020 R2 systems to add additional WebHMI languages that include Spanish, Russian, Norwegian, Portuguese, Polish, Swedish, Italian, German, Japanese.   Simplified Chinese and French were released with 2020 R2
Graphics Migration Assistant v.1 2021-Sep Installation media for Graphics Migration Assistant v.1 that supports thick client to web client graphics conversion for PSO 2020 systems
Common Protocol Drivers (June 2025) 2025-Jun Commonly used protocol drivers for Power Operation as of June 2025