TAC INET Version 2.49

TAC INET Version 2.49

Software Package

Release Date Notes
Software 2017-Jun-20 TAC INET Seven Version 2.49 Host Software ISO
Host software Version 2.49, controller BIN files and user documentation (ISO image).
Software 2017-Jun-20 TAC INET Seven Version 2.49 Host Software ZIP
Host software Version 2.49, controller BIN files and user documentation (ZIP file).
Release Notes 2017-Jun-20 TAC INET Seven Version 2.49 Host Software Readme - Release Notes
Host Software installation requirements, new features, new functions, fixes, corrections and known issues.
Release Notes 2017-Jun-20 TAC INET Seven Version 2.49 Host Software Upgrade - Release Notes
Host Software upgrade instructions, requirements, fixes, known issues.
Firmware 2017-Sep-06 7793, 7798, and 7798C Downloadable Firmware Dated 28 August 2017
Updated controller firmware that provides a fix for a defect that was preventing the proper downloading of doors and points to subLAN devices. The controller firmware revision that introduced the defect was dated 20 January 2017. If you have 7793, 7798, and/or 7798C controllers using that firmware, it is recommended that you immediately update the firmware to this newer revision. 
Manual, Operating Guide 2010-May-01 TAC INET Seven Getting Started
TAC INET Seven System Getting Started, INET Seven System, TCON298, Revision: 05/17.
The following assests are used with TAC INET Version 2.49    
Firmware 2015-Jun-10 TAC Xenta 527 Version 5.1.9 Service Pack A System Program 
Firmware 2015-Jun-10 TAC Xenta 527-NPR Version 5.1.9 Service Pack A 
Firmware 2014-Feb-28 TAC Xenta 527-NPR Version 5.1.9 Service Pack A System Program
Firmware 2014-Feb-28 TAC Xenta 527 Version 5.1.9 Original Language Pack
Firmware 2014-Feb-28 TAC Xenta 527 Version 5.1.9 System Program 
Firmware 2014-Feb-28 TAC Xenta 527-NPR Version 5.1.9
Firmware 2014-Feb-28 TAC Xenta 527-NPR Version 5.1.9 System Program
Release Notes 2014-Apr-16 TAC Vista Version 5.1.9, TAC Xenta 500 700 900 Version 5.1.9 
Firmware 2010-Jan-11 TAC INET MIB