Panel Server Disclaimer

Disclaimer

Starting in May 2025, Panel Server PAS600, PAS600L, PAS800, PAS800L, and PAS800P will be available in two version: Hardware version 1 - HW1 -, and Hardware version 2 - HW2-. Please make sure to download the proper firmware version according to your Panel Server Model.

The Hardware version of your Panel Server is displayed:

  • On the front face of your Hardware, under the MAC and serial number for the Hardware version 2 - "HW: V2.0" - No mention are displayed on the Hardware version 1
  • In the embedded webpages "Maintenance" --> "Firmware Update" --> "Hardware Revision" : "000.000.001" for HW1 and "000.000.002" for HW2

Panel Server Package

Panel Server Package
Software Package Release Date Notes
EcoStruxure Panel Server Entry    
EcoStruxure Panel Server Entry Firmware 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Entry - Firmware Release Notes 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Universal    
EcoStruxure Panel Server Universal Firmware Hardware Version 1 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Universal Firmware Hardware Version 2 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Universal Wired by Design Firmware 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Universal - Firmware Release Notes 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Advanced    
EcoStruxure Panel Server Advanced Firmware Hardware Version 1 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Advanced Firmware Hardware Version 2 2025 - Oct Version 002.004.000
EcoStruxure Panel Server Advanced - Firmware Release Notes 2025 - Oct Version 002.004.000