Search Help




The CO2 + TRH Sensor will help ensure the well-being of your customers, students, or personnel:
All CO2 sensors are maintenance-free in normal environments thanks to the built-in Automatic Baseline Correction (ABCLogic™) algorithm function. The sensors have a life expectancy of 10 years. It requires no calibration, it has a long term stability , and low power consumption.
Monitor indoor air quality, review data on interfacing devices, and control fresh air inside customizable zones.
The wireless CO2 + TRH sensor can be secured directly on a wall or flat surface using double-sided adhesive tape, or by securing the plastic bracket to the wall and mounting the sensor. Using the screws is the recommended method.