Essential Materials
Search Help




→ Connect now to mySchneider to discover the EcoXpert content ←
Exiway Dicube is an addressable system capable of performing automatic tests, generating plant reports and providing supervision of the emergency lighting system. With Dicube you can test and monitor every single connected anti-paninc and exit sign luminaire that can be connected with the Control Unit via a DALI bus protocol. The Exiway Smart Control runs automatic tests, as requsted by EN 62034, centralizing the information coming from luminaires for monitoring and maintenance.
Main advantages

Integration of Ordinary and Emergency DALI luminaires for remote monitoring, automatic test and report management